STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

MTU size and Characteristic size config

Dear ST/forum members,I am trying to configure the BLE slave side. Using latest CubeMx (BLE_Custom.ioc ) and BLE_DataThroughput configuration as reference. My questions:1. CFG_BLE_MAX_ATT_MTU is restricted to 300 in CubeMx? Why is that? Can I make ...

DS.4 by Senior II
  • 3392 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO-WB55RG: As per UM2435, in document mentioned only 1 I2C and SPI. But in STM32CubeMX if check for the same board then it has 2 I2C and SPI

As per the UM2435 NUCLEO-WB55RG board has only one I2C- I2C1 and SPI-SPI1But in STM32CubeMX configuration for the same board it has two I2C: I2C1 and I2C32 SPI: SPI1 and SPI2.Can you please provide more information on this?Thanks!

NK by Associate II
  • 1690 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO WL5 debug problem

Hello to everyone. I am trying to develop an application on Lora on the NUCLEO WL5 series development board. But I could not debug the board via CubeMx. I am trying to use external debugger but I still have mcu not found problem. Can anyone tell me h...

MKoca.1 by Senior
  • 2094 Views
  • 5 replies
  • 0 kudos

Resolved! LRWAN3 - Hard Fault on AT+DR command

Hi everyone,I have a pnucleo lrwan3 kit and I'm trying to setup the end node using the LRWAN NS1 AT Master example from I-NUCLEO-LRWAN package.Everything is working fine until the program gets to the AT+DR command. There a Hard Fault occurs and it ge...

0693W00000GXBx4QAH.png 0693W00000GXBxEQAX.png 0693W00000GXBszQAH.png 0693W00000GXBy2QAH.png
PDevo.1 by Associate II
  • 3165 Views
  • 5 replies
  • 0 kudos

hi I have worked on a project to send audio through BLE with x-nucleo-cca02m2 connected to p-nucleo-wb55 I wanted to know if anyone know how to connect a mems sensor to usb dongle with stm32wb55cgu (UFQFPN48)

The question is how do I connect the output of the pdm and how do I connect the input of the clock to the sensorThis is the sensorsThis is the mcu chip (stm32wb55cgu) Thank you for your supportefiehrman@gmail.com

0693W00000GXVp5QAH.png 0693W00000GXVpKQAX.png
EEhrm.1 by Associate
  • 1068 Views
  • 0 replies
  • 0 kudos

STM32WB5MMG hardware error

Hello,​I am working with a custom board with the STM32WB5MMG SoC and I am receiving a hardware error timer overrun 0x02 after some time. After that the BLE interface stops working.​There is any way to prevent this error? Is related to the hardware de...

FCasa.1 by Associate II
  • 687 Views
  • 0 replies
  • 0 kudos

Zigbee not responding Basic Cluster attributes

Hi,I am working with the STM32WB55 Nucleo board to create a Zigbee device being able to connect to a Philips Hue Bridge v2.1. Using a 2.4GHz sniffer with wireshark I am able to follow the communication which goes through the following steps with no p...

0693W00000DqEUpQAN.png 0693W00000DqEVxQAN.png
JHals.2 by Associate
  • 3125 Views
  • 4 replies
  • 0 kudos

How to debug STM32WB55 Zigbee application ?

Hello,I'm working on a project using Zigbee as main communication network.In this project we develop two devices :One as server and coordinatorOne as client and routerWe based our hardware on STM32WB5MMG.I used the examples of Zigbee_OnOff_Client_Rou...

APEYR by Associate II
  • 8999 Views
  • 17 replies
  • 0 kudos

P-NUCLEO-WB55 RF problem

I have P-NUCLEO-WB55 it worked initially well with BLE stack. Later I have ported Zigbee Stack but things were not working out. I went back and loaded the BLE stack now, but it is not even advertising with p2p sever application. I have tested the GPI...

YSN by Senior
  • 1343 Views
  • 1 replies
  • 0 kudos