STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 132 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4030 Views
  • 0 replies
  • 3 kudos

STM32WB5MMG Zigbee Random Disconnection and reJoin not working

Hi All, I'm currently using an STM32WB5MMG module on two devices to establish a Zigbee connection between them.My project is based on the example called "BLE_Zigbee_Dyn"(one device should also be able t communicate using BLE ) implementing everything...

Jonny by Associate III
  • 2223 Views
  • 2 replies
  • 0 kudos

Zigbee stack crash on Nucleo USB dongle

Hi all,I'm trying to develop on the Nucleo USB dongle. I'm creating an empty Zigbee project with the FW 1.12.1 I configure the minimum in cubeMX the project crash in startup_stm32wb55cgux.s  I'm running FUS V1.2.0.0I'm using the wireless copro : stm3...

0693W00000DpuBJQAZ.png
JFeut.1 by Associate II
  • 1265 Views
  • 1 replies
  • 0 kudos

Can't get an interrupt on Pa7

I'm trying to use Pa7 for an external falling edge irq without success. I have pb1 and pb4 working as expected, but not Pa7. Is there anything special about using EXTI9_5_IRQn vector?

LHarm.1 by Associate III
  • 736 Views
  • 0 replies
  • 0 kudos

STM32WL55 does not receive uart input after a certain amount of time passes after sending RF periodically

Hi I am testing with STM32WL55I programed that MCU transmitted LoRa signal periodically and transmitted data via uart1 periodically.At first, MCU can recieve data via uart1.After a certain amount of time, MCU can't transmitted some bytes via uart1 on...

0693W00000GXDEBQA5.png

MLPF-WB55-02E3 connection to STM32WB55V WLCSP_100.

I have some questions on the response here:https://community.st.com/s/global-search/MLPF-WB55-02E3?t=1636577804470The response references MLPF-WB55-01E3 but I think it should be MLPF-WB55-02E3 for the WLCSP_100 package. Can you confirm the 65 ohm im...

TEben.2 by Associate
  • 652 Views
  • 0 replies
  • 0 kudos

Resolved! Read STM32WLE5C8U6 & STM32WLE4CCU6 UID

Hi,I'm working on the two MCU's STM32WLE5C8U6 & STM32WLE4CCU6 and I need to know the UID in order to indentify each of the products.In the doc it's written that both have UID but there is no address to read them.What I'm missing ?Best regards,

ABric.2 by Associate II
  • 1671 Views
  • 2 replies
  • 0 kudos