STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 227 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4070 Views
  • 0 replies
  • 3 kudos

I got some issues on the P-NUCLEO-STM32WB to upgrade the FUS

Good afternoon,Test1: I want to upgrade the FUS (at the moment it is FUS version 0.5.3.0) to upload next, the FTD thread stack. But when I upload the stm32wb5x_FUS_fw_for_fus_0_5_3.bin (from the last version of Patch-CubeWB: FUS version 1.2.0) with S...

TTAIL.1 by Associate II
  • 2836 Views
  • 6 replies
  • 0 kudos

How to add I2C to I-CUBE-LRWAN SDK SubGHz_Phy example? The reason I'm looking for it is that I was able to run SubGHz_Phy successfully but I'm unable to add the I2C to run successfully.

It's very hard to add it without instructions to not break existing infrastructure with LoRa.When I run simple example generated from classic .IOC file I got the I2C running without a problem.The board I'm using: Murata Type 1SJ

STM32WB5MMG connection couldn't finish

I was testing the STM32WB5MMG on the new U585 IOTA discovery kit and I'm facing some issues.I generated a project using STM32CubeIde with the MXEditor. After enabling all the default peripherals and changing the example config of BLE, some points are...

XPera.2 by Associate
  • 1081 Views
  • 1 replies
  • 0 kudos

"Debugging" crashes program

Running a program on the stm32wl nucleo board works fine, but if I enable debugging it alwaus crashes. This does the same thing on my custom board. It's always the same signal handler

0693W00000KbVNZQA3.png
Bstan.1 by Associate
  • 849 Views
  • 1 replies
  • 0 kudos

Wakeup procedure via BLE for system in low power mode

Hi,I am currently working on a bluetooth application developing it on Nucleo STM32WB55 (FW version V1.13.1, BLE Stack Full).If the system is in a low power state, STOP2, can it be woken up via bluetooth?If so, is this awakening established by any kin...

SDi B.2 by Associate II
  • 1798 Views
  • 1 replies
  • 0 kudos

LoRaWAN Session keys store is already working on V2.1.0 ?

Hello everybody,I'm using the AT code modified in order to join my own server with an OTAA configuration in a solar application, so every morning the system goes up, and late afternoon the system shuts down.I want to store session keys, counters and ...

DPrie.1 by Associate II
  • 845 Views
  • 0 replies
  • 0 kudos