Hi, everyone. Is it possible to build an application that supports all regional standards? AS923-1 / AS923-2 / AS923-3 together are of particular interest (depending on the setting, which is changed via the UART, for example).
The TouchGFXDesigner v4.17.0 will keep freezing. The program does not respond to the mouse and keyboard. When you try to close the program, you are asked whether you want to save the changes, but you cannot do anything or select anything. In this sta...
Hello Romain,I am sending you the requested file attached.I have now noticed that the application no longer freezes. I cannot explain why that is.I am using Windows 10 Pro.