STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! STM32CubeMonitor-RF DLL or CLI

Hi everyone,I am trying to create a windows pc app to talk to the STM32WB board using the dongle.I want to run some scripts, e.g., write to characteristic, connect, read an etc.I saw that STM32CubeMonitor-RF can already run scripts via some text file...

DS.4 by Senior II
  • 1156 Views
  • 1 replies
  • 0 kudos

nucleol073rz's App_eui keeps changing to 0

I'm using nucleo l073rz and I'm trying to connect to Chirpstack.But it doesn't have an uplink. When I checked the JoinRequestMessage, all contents of App_eui were zero. I set it to the original App_eui using the serial port, but it returned to zero i...

0693W00000LwF1OQAV.png
sjung.11 by Associate
  • 1358 Views
  • 2 replies
  • 0 kudos

STM32WL55 MX_IPCC_Init() error from config tool.

On STM32WL55, i have made a skeleton for an app including subghz in fsk, with mx config tool. When building i get an error on one core and warning on the other about MX_IPCC_Init(),wich is declared static in main.c and used in main so i can thing the...

Xynium by Associate III
  • 1671 Views
  • 2 replies
  • 1 kudos

Resolved! OTP area in flash is not empty on brand new STM32WB5MMG

Good day,On a brand new SMT32WB5MMG MCU, I have found that the One-Time Programmable area is not empty. See the image. The OTP area starts at 0x1FFF7000. There is also some data right before the OTP area - what is that doing there as well?For context...

0693W00000LvZmrQAF.png
burn_ by Associate III
  • 5038 Views
  • 9 replies
  • 0 kudos

Resolved! Can't generate code succesfully with CubeMx

Im' following this tutorial of STM32WB55: https://www.youtube.com/watch?v=CKYWy7LKL68&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=19&ab_channel=STMicroelectronicsAll is fine until I try to generate code. It gets stuck at the moment of "Copying libr...

0693W00000Lw9YWQAZ.png 0693W00000Lw9WaQAJ.png
PGarg.1 by Associate II
  • 2054 Views
  • 4 replies
  • 0 kudos