NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I followed the STM32WB Getting Started Series: Part 9 on topic of updating FW to a newer version and reviewed relevant App Notes and HTML from the repository. I use ST-LINK to STM32WB55 Nucleo eval board with STM32CubeProgrammer 2.12.0. The demo code...
I have a previously working app and both examples _EndNode and AT_SLAVE.The board worked well for about 30 hours.I could not get the other 2 examples for this board to compile and work.After a change, neither app joins the network reliably. The gatew...
The sampling frequency is 256kHz, it is an ADC that collects ECG signals.(The question is really not about ADC), what should I belong to with this question?My problem is that the analog signal is output in four channels in parallel after the ADC, whe...
I want to use stm32 to collect ADC digital data. The output of ADC is four digital signals D3, D2, D1, D0 and one clock signal CLK2. I need to add a digital low-pass filter (like fir), how do I collect this 4bit digital signal...Thanks in advance.
I have initialized variable as belowuint8_t u8Flag1ForStoreVer __attribute__ ((section (".RAM1_region")));So, after soft reset I am getting data back.But also same I am getting after hard reset(Power cycle) , even aftre long timeWhat should be value...
I have a working copy of both the ENdNode and Slave applications in cube running on nucleo boardThese both worked from +-20 December to 28 DecemberI then made a small change to the endnode app - I increased the data packet to 50 bytes in lora_app.c->...
I can't find the adc_if.c file for Base Station and Sensor projects in P2P of STM32WL_WS.