Skip to main content
LHP.1
Visitor II
June 1, 2022
Question

Hardfault Handler in STM32WB15 BLE

  • June 1, 2022
  • 1 reply
  • 836 views

Hello.

I am using a NUCLEO-WB15CC board trying to build a BLE application.

I followed the instruction from a YT video by STM: https://www.youtube.com/watch?v=i10X4Blr8ns

I generated code with CubeMX version6-5-0 on linux.

The code called HardFaultHandler() as soon as it reach MX_APPE_Init() in main.c

if i break the while(1) loop in HardFaultHandler, the code continues at __HAL_RTC_WAKEUPTIMER_DISABLE(phrtc) in HW_TS_RTC_Wakeup_Handler() from Core/Src/hw_timerserver.c.

Why is that so? How do I rectify or solve this?

 Below is main.c:

#include "main.h"
 
 IPCC_HandleTypeDef hipcc;
 
RTC_HandleTypeDef hrtc;
 
UART_HandleTypeDef huart1;
DMA_HandleTypeDef hdma_usart1_rx;
DMA_HandleTypeDef hdma_usart1_tx;
 
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_IPCC_Init(void);
static void MX_RF_Init(void);
static void MX_RTC_Init(void);
 
int main(void)
{
 HAL_Init();
 MX_APPE_Config();
 
 SystemClock_Config();
 
 PeriphCommonClock_Config();
 
 MX_IPCC_Init();
 
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_RF_Init();
 MX_RTC_Init();
 MX_APPE_Init();
 
 while (1)
 {
 MX_APPE_Process();
 
 }
}
 
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
 
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
 |RCC_OSCILLATORTYPE_LSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
 |RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}
 
void PeriphCommonClock_Config(void)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS|RCC_PERIPHCLK_RFWAKEUP;
 PeriphClkInitStruct.RFWakeUpClockSelection = RCC_RFWKPCLKSOURCE_LSE;
 PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSI;
 PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE1;
 
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}
 
static void MX_IPCC_Init(void)
{
 
 hipcc.Instance = IPCC;
 if (HAL_IPCC_Init(&hipcc) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
static void MX_RF_Init(void)
{
 
}
 
static void MX_RTC_Init(void)
{
 
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = CFG_RTC_ASYNCH_PRESCALER;
 hrtc.Init.SynchPrediv = CFG_RTC_SYNCH_PRESCALER;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Enable the WakeUp
 */
 if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
void MX_USART1_UART_Init(void)
{
 
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 115200;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_8;
 huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 
 
}
 
static void MX_DMA_Init(void)
{
 
 /* DMA controller clock enable */
 __HAL_RCC_DMAMUX1_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 /* DMA1_Channel2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn);
 
}
 
static void MX_GPIO_Init(void)
{
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
}
 
 
void Error_Handler(void)
{
 
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 

This topic has been closed for replies.

1 reply

Remy ISSALYS
ST Technical Moderator
June 7, 2022

Hello,

This video allows to create an application which run on P-NUCLEO-WB55.Nucleo, so you have to tune it in order to run it on NUCLEO-WB15CC. There is different examples which runs on NUCLEO-WB15CC available in STM32CubeWB package.

Best Regards