STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

SHCI_C2_BLE_Init Fails

I'm trying to start up CPU2 on an STM32WB55. I've looked at various examples and I seem to be doing all the right things. SHCI_C2_BLE_Init returns 0xFF in payload[0] which corresponds to SHCI_FUS_CMD_NOT_SUPPORTEDI have FUS V1.2.0.0 installed and the...

TWood.4 by Associate III
  • 1166 Views
  • 1 replies
  • 0 kudos

Resolved! Programming and Running BLE stack in CPU2

Greetings,Currently the project has a requirement for a Custom BLE server profile. I have a few doubts, for which I'm seeking clarifications.I flashed the 'stm32wb5x_BLE_Stack_full_fw' v1.14 at the specified memory location as per the release notes. ...

ABN by Associate III
  • 2438 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB55 Jump to bootloader problem in P2pClient project

HiI have a strange problem with my p-nucleo board(MB1355C)Using the example as reference DFU_Standalone (STM32Cube_FW_WB_V1.12.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\USB_Device\DFU_Standalone)I am able to jump to bootloader and perform DFU upda...

0693W00000Y6qjaQAB.png
TGUCL.1 by Associate III
  • 1739 Views
  • 1 replies
  • 0 kudos

HSE external crystal issue

Hi team, I am trying to load the program in to the STM32WBRG MCU using ST-LINK/V2-ISOL we are able to succeed the loading and verified the test code using the internal 16MHz RC oscillator, but while using the External 32MHz

na.1 by Associate II
  • 1119 Views
  • 1 replies
  • 0 kudos

STM32 WLJC55 SubGHZ PingPong example (STM32WL Package)

Hello, i got two STM32 Nucleo-WL55JC2 (dual core) and i want to create a radio communication between these two MCUs. I've downloaded the STM32WL Package and i want to upload the pingpong dual core example on my two cards. (I'm using CubeMX 6.7.0 and ...

0693W00000Y707RQAR.jpg
BNamu.1 by Associate II
  • 3111 Views
  • 3 replies
  • 0 kudos