User Activity

Hi all.I'm working on stm32WB MCU, I have a bootloader and an application. The bootloader only check if any update needed and jump to app. When app stops at main I can see that flash status register is set with PGAERR, SIZERR and PGSERR and I have no...
Hi.I'm using stm32wb55 MCU.ADC is running in continuous mode with 6 channels using DMA for the results. I want to use analog watchdog interrupt on just 1 channel that is on rank 2.I have 2 problems, first the interrupts occured only for the channel i...
Hi.I tried to use TAG_OTA_END and TAG_OTA_START from BLE_HeartRate_ota ST project the same it is used in this project to verify the FOTA operation was finished successfully.I added both, PLACE_IN_SECTION in my ble file and also I added this tags in t...
Hi.I can see that CFGBSY bit is set and reset in some MX peripheral init functions, but the main problem is that it stays set after MX_TIM1_Init and it locks my flash for any operation.Did anybody saw this kind of problem?Any help will be appreciate...
Hello.I have noticed that a new FW was released and I tried to update our devices version.First of all, I was working with previous 1.13 version that had BLE stack light, basic and full versions, in 1.15 version I noticed that there is light, full an...
Kudos from