NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I can make the RTC wakeup work in Standby mode, but not STOP2 mode.
i am working with lsm303agr accelerometer and magnetometer sensor module with controller STM32WB , am using the library from the ST for the implementation of software. I can able to fetch data using the I2C protocol. But when I try to use the SPI 3 w...
Hi fellas,We are planning for LoRa based FUOTA updates using STM32 MCUs. The LoRa Transceiver we are planning to use is SX1302. In I-CUBE-LRWAN blog, they told its meant for STM32L0/1/4 series alone. Can we use some other series like STM32G0 series, ...
Hello togetherI am currently doing the tutorial from ST (STM32WB Getting Started Series: Part 12b, Lab. Receiving data from the phone) to send and receive Information with BLE. I am stuck in the video at 15:00 when the device should show up on the ST...
Say I want the Projects/B-L072Z-LRWAN1/Applications/LoRaWAN/LoRaWAN_AT_Slave project loaded up.What exactly am I supposed to do in the IDE?I've loaded that project up, but can only build the debug configuration - it doesn't seem right.I did change th...
There are two inductors, L1 10uH and L5 10nH, in series for SMPS circuit in P-NUCLEO-WB55 design. Why is that? is the sequence affective (smaller L5 coming out of VLXSMPS pin)? Thanks. -wq
I've used BLE for a month now on the wb5mmg with the 1.14.1 firmware with the steval-proteus board. The setup in the .ioc for new projects was always the same:HSEM, IPCC, RCC, RTC, RF, (USART)Activating BLEUsing Default P2P Settings or Custom Templat...
My configuration is when button is pressed start advertising and stop advertising after 100ms. When the button is pressed a few times device gets hung and continuously advertises.When I tried debugging following is the traces I didn't understand thi...
Hello,we’re doing some research on LoRa tecnology to evaluate if it’s suitable for our products. We’re interested in STM32WLxx MCU, so we downloaded STM32CubeWL Firmware package from GitHub.We are trying to understand the principle of working of some...