User Activity

Hi, Context:I am currently developing a LoRa board implementing the STM32WL55. I didn't get the SubGHz Middleware to work, so i implemented the approach as detailed in the reference manual page 206. The code compiles, and the tx-complete interrupt is...
Hi,i am working on a Project right now where i need to send some data via LoRa. I'm using a STM32WL55 and i had some trouble with the radio setup, so to check the basic functionality of my radioi rebuilt the SUBGHZ_Tx_Mode example for my board and co...
Hi, i'm currently working on a Project where i need to send some data via LoRa.I've been struggeling to get a transmission going, so i decided to check the basics.To test the radio, i went ahead and rebuilt the SUBGHZ_Tx_Mode example from the STMCube...
Hi, im currently working on a project (STM32WL55) where i need to send data via LoRa. I plan to use the SubGHz HAL driver as it seems pretty low level and provides easy usage of the internal subghz spi.While researching, i found AN5406 where it says ...
Hi, im currently working on a project for universtiy and im quite new to stm32. I hava a sensor on my board that coummuicates via UART, were it dumps its data once per second. My problem is that the first HAL_UART_RECEIVE works as intended, but after...
Kudos from