STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

De-whitening, endianess and length issues

I am trying to use the WL55 with a legacy 2-gfsk system that relies on CC1120 chip. The major issue here is related to de-whitening of the received data. I am editing the subghz ping pong example. Band, AWG and datarate are coherent with the legacy s...

ltoso.1 by Associate II
  • 1037 Views
  • 0 replies
  • 0 kudos

RAK3172 LPUART sample code-LED not litting?

I am checking the below example code given in RAK3172 low level development folder.C:\en.stm32cubewl\STM32Cube_FW_WL_V1.0.0\Projects\NUCLEO-WL55JC\Examples_LL\LPUART\LPUART_WakeUpFromStop_InitThe only change I made here is for LED2 , GPIO pin changed...

PP.3 by Associate
  • 1311 Views
  • 1 replies
  • 0 kudos

STM32WLE5 wake up from stopmode using LPUART with LSE

Hello, to get a lower power consumption in my application i would like to go in stop mode 2 and wake up shortly to receive some characters on the LPUART. But unfortunately my mcu does not wake up. I can see with the debugger that the send Byte is in ...

APell.3 by Associate
  • 1223 Views
  • 0 replies
  • 0 kudos

Sigfox communication through arduino IDE with STM32WL55

I would like to create a script by arduino IDE that allows me to communicate in Sigfox. I own an STM32WL55. I haven't found any library on the internet that allows me to do this communication. Is there any documentation explaining how to program this...

JOliv.10 by Associate
  • 1604 Views
  • 1 replies
  • 1 kudos

Resolved! Why doesn't this simple openthread project work?

Hello, I am trying to create a simple openthread project on my NUCLEO-WB55RG. There is no custom code in this project; just the code generated from the CubeMX ioc file attached.By all means, I think that I have all the necessary settings for this pro...

CMasc.1 by Associate II
  • 1747 Views
  • 2 replies
  • 0 kudos