STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 227 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4069 Views
  • 0 replies
  • 3 kudos

Bug for BLE Init in new wb5 firmware 1.15

I've used BLE for a month now on the wb5mmg with the 1.14.1 firmware with the steval-proteus board. The setup in the .ioc for new projects was always the same:HSEM, IPCC, RCC, RTC, RF, (USART)Activating BLEUsing Default P2P Settings or Custom Templat...

0693W00000WKe8SQAT.png
Lotta by Associate II
  • 6422 Views
  • 13 replies
  • 0 kudos

STM32CubeWL v1.3.0 - General questions on the examples

Hello,we’re doing some research on LoRa tecnology to evaluate if it’s suitable for our products. We’re interested in STM32WLxx MCU, so we downloaded STM32CubeWL Firmware package from GitHub.We are trying to understand the principle of working of some...

0693W00000aJeCYQA0.jpg 0693W00000aJeCdQAK.png
GGhet.1 by Associate
  • 1737 Views
  • 1 replies
  • 0 kudos

Resolved! The simplest and most basic LL driver App doesn't work

We tried the simplest and the most basic LL driver based App, LED blinking, on Nucleo boards:int main(void) { LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG); LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR); NVIC_SetPriorityGrouping(NVIC_PR...

WQ by Associate III
  • 5299 Views
  • 11 replies
  • 0 kudos

How create devEUI for public Lora network?

I have one product with inside the module Murata CMW. The product will be present on a public Lora network. The product is a sensor, so it will trasmit dataI need to go in mass production and I need to create the devEUI for each deviceHow I can creat...

FSogn by Associate
  • 2308 Views
  • 2 replies
  • 0 kudos

STM32WL55 as single chip 4-fsk transceiver

Hi, I'd like to understand how I can setup the semtech transceiver to work with 4-FSK modulation. I configured a project in cube mx but I have doubts on the bandwidth and datarate parameters.I know that my datarate is 9600 bps, then bandwidth and cod...

ltoso.1 by Associate II
  • 2303 Views
  • 2 replies
  • 0 kudos

MOOC - STM32WL workshop - 4 Point to point

First of all, I was doing basic HAL_UART communication with lora modules. Now I have a new project which requires really really low power so I decided to go with stm32wl.I will have 50 end node device (sensor device) and 1 base station. Sensor device...

AHakk.1 by Associate III
  • 1170 Views
  • 1 replies
  • 0 kudos

STM32WLE5 'Failure To Execute Command'

I am experimenting with the STM32WLE5 and the embedded SX126 LoRa-radio. (aka SubGHz)I simply reset the SubGHz, then read its status, and this always returns a 'Failure To Execute Command' (according to section 13.5.1 GetStatus from SX126 datasheet) ...

Strooom by Senior
  • 4233 Views
  • 6 replies
  • 0 kudos