2022-09-14 3:19 AM
Hi,
im currently working on a project (STM32WL55) where i need to send data via LoRa. I plan to use the SubGHz HAL driver as it seems pretty low level and provides easy usage of the internal subghz spi.
While researching, i found AN5406 where it says in page 6 that i need to implement the HAL_SUBGHZ_MspInit function, but not how.
In stmwlxx_hal_subghz.c there is a weak function that doesn't do anything, and is meant to be overwritten:
/**
* @brief Initialize the SUBGHZ MSP.
* @param hsubghz pointer to a SUBGHZ_HandleTypeDef structure that contains
* the handle information for SUBGHZ module.
* @retval None
*/
__weak void HAL_SUBGHZ_MspInit(SUBGHZ_HandleTypeDef *hsubghz)
{
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_SUBGHZ_MspInit should be implemented in the user file
*/
/* Prevent unused argument(s) compilation warning */
UNUSED(hsubghz);
}In HAL_SUBGHZ_Init it says that the function is meant to Init the low level hardware : GPIO, CLOCK, NVIC...
/* Init the low level hardware : GPIO, CLOCK, NVIC... */
HAL_SUBGHZ_MspInit(hsubghz);I initialise the hse, and the Subghz radio interrupt via MX, so
my question is, which low level hardware needs to be initialised in HAL_SUBGHZ_MspInit for the subghz radio to work.
2022-09-14 9:18 AM
Hello @D.Heink ,
You need to enable the SUBGHZ SPI clock and to initialize the radio interrupt.
You can fin an example of LoRa communication in the STM32Cube_FW_WL_V1.2.0, under "Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy\SubGHz_Phy_Per". This example use only the LoRa communication so it can help you to configure your project !
I hope this helps you !
Regards
Louis
2022-09-15 1:11 AM
Thanks!
2022-09-15 1:25 AM
But doesn't the SubGHz_Phy_Per use the GFSK modulation?
Also, the SubGHz_Phy_Per doesnt employ the SubGHz HAL driver instead it uses the SubGHz_Phy middleware. So i can't use it as a reference.
2022-09-15 3:54 AM
Okay, i read the section of AN5406 again, and realised that it does indeed give an explanation on how to implement the HAL_SUBGHZ_MspInit() function.
PWR: Enable wakeup signal of the sub-GHz radio peripheral.
I couldn't find what the wakeup signal of the sub-GHz radio peripheral is, can can somebody give me a hint?
Further i found that there is already a HAL_SUBGHZ_MspInit() overwrite where the interrupts get setup so that probelm is solved.
@Louis AUDOLY The SUBGHZ SPI clock is derived from the PCLK3 according to RM0453 page 300. Isn't it enabled with the normal clock initialisation from mx? If not where do i need to enable it manually?
2022-09-15 5:50 AM
Nevermind, i found the SUBGHZ_Tx_Mode example and that answeres all my questions.