User Activity

Hi, I'm using the APP_LOG function to print data to serial. Here's how i do it:APP_LOG(TS_OFF, VLEVEL_L, "%d,%d,%d,%d,%d,", front_brake_pressure, rear_left_wheel_speed, rear_right_wheel_speed, front_left_wheel_speed, front_right_wheel_speed);APP_LOG(...
Hi all,I am receiving date and time by CAN for my application, and not using the RTC functionality because I couldn't get it to work with LoRa.Basically I receive day and month separately, and declare the year as a int. Same thing for the time, I rec...
Hi all,I'm trying to use Timer16 to create a 50Hz timer to save files in the SD card. I managed to make the timer work blinking a LED, but when I put the code to save it only saves one line. Here's the logic:First I create a file  and initiate the ti...
Hy guys, I want to be able to create a named file in an SD card based on how many files I have in the directory, per example: if I have only 1 file "file1", I'll create the next one as "file2". I searched the ff.h library, but didn't find anything th...
Hello guys!I'm working with STM32WL series using the LoRa application, for that the RTC must be in binary mode.However, I need the calendar and timestamp for my project, which implies that I need to use BCD mode.I'm aware that the RTC3 has the mixed ...