NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Is it possible to create a project in CubeMX for a concurrent BLE & Thread application for the STM32WB55?My attempts so far only allow for either a BLE or a Thread project (not both together).Thanks
When I create a new project using STM32CubeMX with my board (NUCLEO-WL55JC1), neither defines for PIN labels will be generated in main.h nor is there a BSP folder in the Drivers folder with a xxxnucleo.h containing definitions as I have seen in the e...
Hello,I am trying NUCLEO-WB55RG Matter device over thread example with apple home pod mini (support thread border router and matter) but it fails to commission and connect.I have already flashed "STM32WB_Copro_Wireless_Binaries/STM32WB5x/stm32wb5x_BL...
While reverse engineering a demo application from ST / Seeed ( Seeed-Studio/LoRaWan-E5-Node at qian (github.com)), I started monitoring all commands and register access from the MCU to the embedded SX126.I see there are writes to register:WR [08E2]:0...
Ive seen this issue in various different forms over the last 2 years and it seems like CPU2 is corrupting the TL_RefTable structure while configuring advertising. We are using v1.15.0 of the stack on a STM32WB55. This happens every few hours in the f...
Hi! I have a peripheral that callsaci_gap_terminate(BleApplicationContext.BleApplicationContext_legacy.connectionHandle, HCI_AUTHENTICATION_FAILURE_ERR_CODE)aci_gap_terminate(BleApplicationContext.BleApplicationContext_legacy.connectionHandle, HCI_AU...
The new STM32WBA series comes to complete the STM32 Wireless MCUs portfolio. The STM32WBA series is brings designers the performance, efficiency, and security required for Bluetooth® Low Energy 5.3-enabled applications. Certified for Bluetooth® Low...
Can you point me to any wireless module out there (WiFi, Bluetooth, Zigbee, whatever).Requirements:Has easy integration with any stm32 MCU with examples in STM32CubeIDE and preferably some community support. I need the chosen protocol to offer certif...
I have NUCLEO-WB%55RG the VREF+ and VDDA are connected together. Can I use the 2.5V internal VREF for the ADC please?