STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

How to use Temperature Measurement Cluster with ZigBee?

Hi,how can I use the Temperature Measurement Cluster with Zigbee? I have configured STM32 CubeMX with an endpoint and the cluster, but "zcl.temp.meas.h" doesn´t contain functions for handling the cluster. Only "ZbZclTempMeasClientAlloc" and "ZbZclTem...

Kampi by Associate III
  • 1526 Views
  • 1 replies
  • 0 kudos

Resolved! Why does the LoRaWAN_End_Node example project not run when debugging on my STM32WL55JC Nucleo-64 board ?

The example project shown below builds and downloads successfully and halts at main(). The ST-LINK appears to connect and start successfully. It is when I click on run that the ST-LINK server says "Target is not responding, retrying..."I changed abso...

0693W00000JNpsGQAT.png 0693W00000JNppgQAD.png 0693W00000JNq1DQAT.png 0693W00000JNq26QAD.png
MRubi.2 by Associate II
  • 4194 Views
  • 7 replies
  • 0 kudos

Resolved! Which pins can I use as ADC in B-L072Z-LRWAN1 board?

Hi everyone!I need to have several pins acting as ADCs to get data from different analog sensors connected at the same time. In board's datasheet I see that this board has 1 ADC with multiple channels (12 channels to be precise).The problem is that C...

pbdiazam by Associate II
  • 4344 Views
  • 8 replies
  • 0 kudos

Resolved! STM32WB tBleStatus values

Hi,This is my architecture:1 board client.5 board servers.In the client i have:A routine that try to connect, pair and update MTU size of all the servers.A routine that send and receive message from the paired servers.Right now i have some problem be...

LSpad.1 by Associate III
  • 2415 Views
  • 3 replies
  • 0 kudos

Resolved! ASTRA1B console output

I am evaluating the ASTRA1B demonstration board. I powered up the board, with factory firmware, via USB and attached an STLINK-V3MINIE debugger/programmer to the J300/STDC14 connector on the expansion board to a PC running TT.Output to console worked...

david368 by Associate II
  • 4712 Views
  • 1 replies
  • 0 kudos

LoRaWAN FUOTA example migrate to STM32WLE5

 HiI'm trying to migrate and run LoRaWAN FUOTA example on STM32WLE5 custom hardware. I tried to use solution from: https://community.st.com/t5/stm32-mcus-wireless/how-to-migrate-from-stm32wl55-to-stm32wle5/m-p/190815but replacing STM32WL55JCIX_FLASH....

flash_write_fix.jpg error1.JPG error2.JPG
meloon by Associate II
  • 7281 Views
  • 9 replies
  • 7 kudos

Resolved! High speed GPIO switching

Hi. Everyone.I'm trying to control external MUX using a GPIO pin in the STM32WB55 microcontroller.Because of a limited number of PWM pins, I'm trying to use a GPIO pin for continuous regular switching.My question is that even though the company said ...

KKIM.6 by Senior II
  • 3196 Views
  • 3 replies
  • 3 kudos

Resolved! STM32WB55 - Where the value is stored?

I have stm32wb55 , i have created a service using stm32cubeIDE, in that i have like 3 characteristics  1:: myChar, 2: mynotify and 3: mywrite,, ( mynotify has nothing to do with this problem). mychar is used to read the value only and mywrite is set ...

SikandarLF_0-1697705560484.png