About example code of FSK communication with STM32WL55
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-11 9:30 PM
Hi
I want to do FSK communication using STM32WL55.
Each version I have installed is listed below.
- Firwmare : STM32Cube_FW_WL_V1.3.0.
- STM32CubeMX : 6.8.0
- STM32CubeIDE : 1.12.0
It seems that the settings etc. have changed a lot from when firmware version 1.1 was used. Previously it was a single core setup, but the current version is a dual core setup.
Please find example code for fsk communication with dual core configuration.
Thank you.
Labels:
- Labels:
-
STM32Cube MCU Packages
-
STM32WL series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0