NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I found the DMA request mapping of the F4 series on ST's official website. With this form, I can configure DMA on zephyr. My problem is that I cannot find the DMA request mapping of STM32WBA52CG. Can you provide me with one? Thank you.The device tree...
ADS1219 Data SheetHello, I am attempting to communicate with TI's ADS1219 via I2C from a STM32WL55JCI, I know the I2C works becuase I can use the same line to write/read from a FRAM chip. Unfortunately, the ADS1219 communication always results in a H...
Hi,I am a bit confused about re-join request process on the lora STM32WL. I want to make my end node will join request to the gateway for five times when the join accepted process is not happening. After five times the join request process and end no...
Hello I have two STM Nucleo-WL55JC2 boards. I have tried running the SubGHz_Phy_PingPong example and it works flawlessly. When observed using TeraTerm, I am only able to see the RSSI and the SNR values. I also need to observe the latency of this ...
Hi, we are using stm32wb55 board for wearable project. logs on serial port are fine when we flashed simple hello world program in loop. But when flashed the application menu developed by us we are seeing some junk value all the time. we are setting t...
Hello, I am trying to figure out a root cause for a weird unexplainable error on STM32WB with BLE Stack. In our application, we have BLE stack fully functional, but every now and then, when we make a small change, like adding a debug line, APPE_SysUs...
Hey,Im working with nucleo-wl55jc1 and I’m trying to work with 300kbps rate.I’ve read in the RM0453 reference manual that it is possible, but as I know the gfsk parameters doesn’t allow this rate.Can someone recommand gfsk parameters that work will w...
this is the example of BLE heart rate ,its working and showing data on ST BLE Sensor app.The data that is taken in the program is raw .i want to print data of ADC channel .how i can assign the ADC channel data to the app or how i can replace the ran...
Hi, I am using two NUCLEO WB15CC boards to make the BLE p2pcentral and BLE p2pServer work as said in the ReadMe of the these examples. But I always run into the same error on the client side. I am using the latest firmware on both sides. From the deb...
Hello, It is not clear to me if I can set stm32wb55 to advertise for connection (e.g., fast, slow) during sleep mode.In case a client connects to me, will I get a connection event that will wake CPU1?What are the sleep modes( power consumptions) of ...