STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 227 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4070 Views
  • 0 replies
  • 3 kudos

Resolved! Low Power Run Mode in STM32WBxx

I want to know if the STM32WB series can operate normally with a main frequency of 100 kHz in low-power-run mode, including the RF part? 

DaveGoing_0-1703062439587.png
DaveGoing by Associate II
  • 1671 Views
  • 1 replies
  • 1 kudos

Resolved! How to use STM32WB5MM-DK?

Hi,It's first time using st product to me.according to that's UM, i thought that connect CN11 to PC it work debugging.but it wasn't and showed warning message "No ST-LINK detected! Please connect ST-LINK and restart the debug session"ST-LINK isn't in...

Cannot send more notifications

I have just sent a notification to the client,  but noticed , I did not get a notification confirmation event back.This event :(ACI_GATT_SERVER_CONFIRMATION_VSEVT_CODE) Since then, I cannot send any more notifications on the characteristic. Why is th...

DS.4 by Senior II
  • 874 Views
  • 0 replies
  • 0 kudos

External clock instead of oscillator

Hi,currently, I am using an NX2016SA (as recommended by ST) to generate the HSE (32 MHz) for an STM32WB55RGV6 microcontroller.I did not calibrate it, but so far everything works and I have a BLE range of up to 25 meters.Now I am planning to getting m...

RWeil.2 by Associate III
  • 9276 Views
  • 13 replies
  • 1 kudos

SMPS - Danger the device may be destroyed

Hi all,I read this advertising in the datasheet:<<The SMPS needs a clock to be functional. If for any reason this clock stops, the device maybe destroyed.[...]Danger: Before enabling the SMPS, the SMPS clock detection must be enabled in the sub-GHz r...

Stm32wb55rev6 communication with custom zigbee3 client

I have a zigbee 3 client working on channel 11 . But It was developed by some other person who was not in touch anymore .. the issue is I need to develop a project that only read a temperature data and frequency value and send those 2 values over zig...

niko27 by Associate II
  • 1338 Views
  • 1 replies
  • 0 kudos

Trying to interface with STM32WB on B-U585I-IOT02A

Hello,I am trying to comunicate the STM32U5 of the board with the STM32WB module, as I need a star network (1 client with 5 servers), I could also use a mesh. To comunicate different nodes. I am having trouble with it, as I just send basic "AT+BLE_RS...

VCasa3_0-1702673869786.png
VCasa.3 by Associate II
  • 1243 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB and BlueNRG-1 Compatibility Using ST Drivers

Hi, I'm working on a project involving 2.4GHz RF communication and I am considering using the STM32WB series alongside the BlueNRG-1. I'm looking into the compatibility of these two devices, especially regarding the use of ST's specific drivers. My q...

pedsa by Associate
  • 2566 Views
  • 1 replies
  • 2 kudos

Migrate from SPBTLE-RF to the STM32WB1MMCH6

Looking to migrate our design from the SPBTLE-RF to the STM32WB1MMCH6.  Our application is running on a separate MCU communicating with the module using the HCI & ACI doing BLE communications.   Has anyone done this migration, or know if the modules ...

stst9181 by Associate II
  • 781 Views
  • 0 replies
  • 0 kudos