STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

BLE lost packets in high througput app

Hello!I am having trouble with lost BLE packets in my system:- TX: STM32WB15CC- RX: nRF52840I have tried so many different things to patch this, but I continue struggleling. For my app, I get a 247B frame ready to be sent every 3ms, so I need a high ...

aarnaizz by Associate
  • 1175 Views
  • 1 replies
  • 0 kudos

UTIL_SEQ_SetTask after pause not working

Using Nucleo-WB55 and I call the above command.  I put a break point and can see then later that I call UTIL_SEQ_SetTask with the same mask HOWEVER I never go back into my function.  Can anyone tell me what I am doing wrong?

SWenn.1 by Senior III
  • 853 Views
  • 1 replies
  • 0 kudos

Resolved! BlueNRG-M2

Hello,actually, i'm using the bluetooth module BlueNRG-M2 , and i want to know the communication distance in meter please and the length of the antenna .Thank you 

ljm by Associate III
  • 3022 Views
  • 7 replies
  • 0 kudos

STM32WB custom_app.c vs custom_stm.c

Hello....I have generated code with CubeMX for the WB55.  I have read and write on some characteristics with some require authentication.  On one characteristic I have read, write (with authentication) and notification set.  On this same characterist...

SWenn1_0-1708979653285.png
SWenn.1 by Senior III
  • 1266 Views
  • 1 replies
  • 0 kudos

STM32WB5MMG - CPU2 is Blocking Flash operations from CPU1

Hi everybody,Here's a bit of context of my project:I'm using BLE Mesh Template, using Sensor and Generic Models.I'm enabling the USB and the CDC middleware. Thus:I changed the configuration of the SystemClock.The nodes are mostly self-provisioned.One...

rdiaz_ice by Associate II
  • 2040 Views
  • 2 replies
  • 0 kudos

STM32WB1MMC antenna

Hello, is there anything which specifies exactly the copper restriction area (page 11) under the antenna? Thankshttps://www.st.com/resource/en/datasheet/stm32wb1mmc.pdf

marc6h by Associate
  • 804 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB5x battery-powered BLE device - missing low power APIs?

Dear all,we are trying to build a simple battery-powered BLE device. It should basically measure at intervals and advertise results only (minus the occasional update connection). With limited power resources we would expect to shut down both cores an...

SVogl.1 by Associate II
  • 3825 Views
  • 6 replies
  • 0 kudos