STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! Can someone explain the function of SX_FREQ_TO_CHANNEL?

Hello,I'm working on an application that uses the NUCLEO-WL55JC development board. I was looking in the SubGHz_Phy_PingPong example code, and I noticed a macro called SX_FREQ_TO_CHANNEL. To use this macro, it seems you input the carrier wave frequenc...

AJ_1 by Associate III
  • 3267 Views
  • 7 replies
  • 3 kudos

Resolved! STM32WLE5JC Receiver Chain

Hi !   I read the datasheet, and it says: "The receive chain comprises a differential low-noise amplifier (LNA), a down-converter tolow-IF by mixer operation in quadrature configuration". 1. What is the GAIN and the NF of the diff. LNA ?       1.a Is...

KTrot.1 by Associate II
  • 1384 Views
  • 1 replies
  • 0 kudos

Resolved! Creating a LoraWAN server on an stm32 chip

I am making a device that is to take pulse outputs which have been converted to wireless LoRaWAN signals, and convert it back again into a hardwire pulse output. For the receiving device, I intend to use a modem board PN 109990166 connected to an STM...

How to calculate impedance matching for STM32WLE5 RF network?

I am attempting to compute an impedance matching network by following the guidelines outlined in the ST Application Note - AN5457.However, on page 24, the formula and calculations appear unclear to me due to the presence of a negative value under the...

Levan_2-1707896427471.png Levan_3-1707896650413.png
Levan by Associate III
  • 2044 Views
  • 1 replies
  • 1 kudos

Resolved! BWB1MPAN1

Hi, the problem is very simple, yet I haven't seen any information about this case in the foro or anywhere.When trying to build the example proyect BLE_HR_p2p_Sensor which I think was already in the B-WB1M-WPAN1 board relesed to start cathing up with...

MST1 by Associate
  • 1660 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB55 Sending notification to phone

Helloi have been following the stm32wb55 getting started, i have been successful in lab 12b about sending from the phone to the board. working with 12c has not been successful, am pressing the button but i dont receive a notification on the phone but...

1713519417014.jpg gatt.png permission.png property.png
PMato.1 by Associate II
  • 1420 Views
  • 1 replies
  • 0 kudos

Resolved! WBA55_P2P_SERVER_WORKSHOP

Hello everybody!I installed STM32CubeIDE 1.15.0 and I tried to follow the session STM32WBA5x workshop - 3:https://www.youtube.com/watch?v=BLs1KzC-s4obut STM32_WPAN is in grey; explanations say me to install other things, but it seems boxes insides ot...

Mirko74 by Associate
  • 979 Views
  • 1 replies
  • 0 kudos

STM32WB missing HCI_LE_CONNECTION_UPDATE_COMPLETE _EVENT

I have been testing with two STM32WB boards, one as central and the other as peripheral. I read in the document "Building wireless applications with STM32WB Series microcontrollers" (newest member cannot add links so I could only paste the title of t...

HLin.3 by Associate II
  • 2156 Views
  • 3 replies
  • 0 kudos