STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! MuRata CMWX1ZZABZ Variants

Hi,Many of the MuRata CMWX1ZZABZ variant support "Opne MCU" such as the -078 variant; meaning the STM32 chip is programmable. Appearently some do not have the "Open MCU" feature even though they use an STM32. Was hoping someone could clear why this i...

Resolved! Master and Slave Project on B-L072Z-LRWAN1

I'm new to the ST development Environment and it is my first time to be using embedded systems. My aim is to make a project of one master that communicate with multiple slaves. I have already tried the ping pong example with 2 B-L072Z-LRWAN1 boards a...

Sondos by Associate II
  • 2467 Views
  • 4 replies
  • 1 kudos

Resolved! STM32WB p2p Client could't p2p Server?

   Initially Iam flash 2 binary files to STM32WB5MMG (stm32wb5x_FUS_fw.bin & stm32wb5x_BLW_Stack_full_fw.bin ) in that case p2p Server works with ST BLE Toolbox in mobile but in my project p2p Client as another MCU.p2p Client not working well its can...

Kavinraj by Associate III
  • 2281 Views
  • 4 replies
  • 0 kudos

Sync Word for Modem Lora

 Hello ST Community,I am currently working with a STM32WL 55JC  and I need assistance with setting the sync word for both the transmitter and receiver. Here are the details of my setup.Here I have configured my module to USE_MODEM_LORA and these are ...

doubt1.JPG doubt2.JPG doubt3.JPG doubt5.JPG