User Activity

Hello,I'm using BLE_p2pClient and BLE_p2pServer programs.I had pairing request in BLE_p2pClient to have both devices bonded.Now, I want to have a fast connection between client and server; actually, the connection between client and server is about 2...
Hello,I'm trying to flash \STM32Cube_FW_WB_V1.18.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x\stm32wb1x_BLE_Stack_full_fw.bin at address 0x08021000 with SMTCubProgrammer version 2.14.0I think that it is unsuccessful, and the application BL2_p...
Hello,What I have done:- Following instructions from AN5185 document.- Using STM32CubeProgrammer v2.14.0- NUCLEO-WB15CC powered on- With STM32CubeProgrammer :- ST-Link configurationST-Link upgrade (v3.12.3)Update to firmware V2J42M27- ST-Link Connect...
 Hello,I am downloading the firmware \STM32Cube_FW_WB_V1.17.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x\stm32wb1x_BLE_Stack_full_fw.bin to the STM32WB15CC using STM32CubeProgrammer v2.14.0, with USB cable.At the end, I have :    11:21:53:481...
Hello,I'm writing an application running on Windows and Linux, using Qt to update STM32WB15CC application.I have read AN5247 document and implement it, but my Qt application never receive the last Reboot Indicatatione ( characteristic uuid: "{0000fe2...