STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 135 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4032 Views
  • 0 replies
  • 3 kudos

Resolved! S2-LP searching for library and examples

Hi, where can I find the S2-LP chip library and examples on C. Also does STM provides any protocols with open code for frequency hopping and mesh based on sub-1 GHz external radio chip?  I've found just sw package with gui to configure radio S2-LP an...

AKali by Associate II
  • 1614 Views
  • 1 replies
  • 0 kudos

Resolved! Error: FUS_STATE_ERR_UNKNOWN: Unknown error

Hello, I am using a P-NUCLEO STM32WB Bluetooth 5 and 802.15.4 Nucleo Pack including a USB dongle.While trying to update the FUS of the USB Dongle to set up a Thread network, I encountered several errors.Initially, I was able to connect in DFU mode, b...

Screenshot 2024-05-22 143244.png Screenshot 2024-05-22 143334.png Screenshot 2024-05-22 143537.png Screenshot 2024-05-22 144025.png

LoRaWAN_End_Node_DualCoreFreeRTOS stops transmitting

I have a "working" demo of the LoRaWAN_End_Node_DualCoreFreeRTOS. I have it connected to a gateway and see a new payload every 10 seconds as expected. However, it stops transmitting after so long (usually 2-3 minutes). All I can tell is I get an I...

AParr.2 by Associate
  • 1077 Views
  • 1 replies
  • 0 kudos

MCU STM32WLE5 radio wake-up reason

Hi, For my project I need to put a MCU STM32WLE5CCU6 in standby mode and configure several wake-up type : Wake-up pin 1 on PA0RTC wake-upRadio wake-up on a LoRa message received by the embedded Sub-GHz radio module of the MCU with the bit EWRFIRQ (re...

STM32WB35 Custom Server APP & LPWR connection

I've try and I think I understood STM32WB HeartRate Exemple and on a Nucleo board it works perfectlyI can go to stop2 and keep active advertising on CM0 and keep being connectable and it wakes CM4 when connection happensbut when I try on my own app i...

oga_0-1714146022006.png oga_1-1714146134990.png
oga by Associate III
  • 1552 Views
  • 2 replies
  • 0 kudos