STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 131 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4020 Views
  • 0 replies
  • 3 kudos

How to factory reset ASTRA1B

Hi,Bought online  ASTRA1B  previously used,  for school project,I do not have experience with  ST Boards.Need Help with following:where to find stock firmware (default factory firmware)  ?Do I need STLINK-V3MINIE for flashing firmware ?How to factory...

Resolved! Costum board stuck at PeriphCommonClock_Config();

hi, Im using my own costum board with a STM32WBA52CG on it. When I'm nog using the RF my code is working perfectly. When I activate the RF in the STM32CubeIDE, my code is stuck in  PeriphCommonClock_Config();More specifically in the following code: I...

Screenshot 2024-05-07 at 17.34.13.png
matsmort by Associate II
  • 2468 Views
  • 4 replies
  • 0 kudos

HCI_COMMAND_COMPLETE_EVT_CODE cannot be received

BLE peripherals are implemented using NUCLEOWB55RG.I would like to check if Advertsing is working properly by receiving the completion of the asynchronous aci_gap_set_discoverable execution with HCI_COMMAND_COMPLETE_EVT_CODE, HCI_COMMAND_COMPLETE_EVT...

STM32WL DAC Sample-And-Hold: Internal capacitor?

I want to generate a constant, steady voltage as COMP INPM in STOP1 with the DAC (using HAL libs at the moment).Unfortunately I cannot get a steady signal. The voltage drifts around some seconds, stabilises and starts from the beginning (oddly seems ...

surumadurum_0-1713209445540.png

SIGFOX_API_start_continuous_transmission

Using this API returns 0x3157 error code after running SIGFOX_API_close successfully (return code is 0), anyone tried that? What are we missing here?BTW - Same behavior observed when using ST provided Sigfox_AT_Slave_DualCore example out of the box w...

ASchw.1 by Associate II
  • 2149 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WL55 dual core debug _ error 18 when debugging CM0+

Hello,I have started to use stm32wl55 nucleo.I try to debug a basic application.I start by debugging CPU1 (CM4) than after booting CPU2 (CM0+) i run the debug for the second CPU.But ST-LINK: Could not verify ST device!error details :Error in final la...

malarab by Senior II
  • 15775 Views
  • 16 replies
  • 0 kudos