User Activity

Good morning,I have been following the stm channel board videos on the LoraWan examples. I was able to correctly configure and connect the board from the example provided in the MX “LoRaWan_EndNode”.But replicating the last video:https://www.youtube....
Good morning,I am using an STM32 WL55JC1 starting from the end node example.I am unable to figure out in the code how to set how long or how many tries it makes before it stops trying to connect to the gateawy.Could you please point me to this inform...
Good morning,I am building a system with stm32 wl55jc1 to count water flow with a pulse flow meter.So I created two internal clocks in stm32 one to create a time window and the other that counts each pulse received from the sensor. At the trigger of ...
Good morning,I am creating an application that would require the use of several stm32wl55.The idea is to have one microcontroller configured as a LoraWan EndNode communicating with TTN and a set of Slaves communicating via subghz (which will be slave...
Kudos given to