STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Why can't I get a value near 2048 with ADC(12Bit)?

I have an issue where I can't obtain values near 2048 in the 12-bit ADC sampling of stm32wb5mmg. The actual data is shown below. hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; hadc1.Init.Resolution = ADC_RESOLUTION_12B; ...

ADC.png
TH5 by Associate II
  • 1874 Views
  • 4 replies
  • 0 kudos

[ STM32WB5MMG ] : CPU2 stuck in non discovery state....

Hi, I have a custom board with a STM32WB5MMG module.This board is very simple. It is a Bluetooth dongle which act as an intermediate between and a serail bus for an other board.In some case, almost one time in 10, at power up, the dongle still stuck ...

arault by Associate II
  • 1423 Views
  • 1 replies
  • 0 kudos

STM32WB RSSI reporting

Dear ST experts,I am developing a Zigbee wireless solution where I have a coordinator and several Zigbee routers and end devices from different manufacturers. My coordinator is a HMI, and one of its capabilities is to display the connection quality o...

d-serj by Associate
  • 2139 Views
  • 3 replies
  • 0 kudos

Resolved! STM32WB55CGU6 Radio configuration

Hi to allI got interested on STM32WB55CGU6 which is recently available as a development board found online and in its reference manual I kind of notice that there is no detailed explanation or rather configuration for the Radio CTRL register and BLE ...

Rashid by Associate
  • 2217 Views
  • 2 replies
  • 0 kudos

Resolved! UART NOT WORKING IN SEQUENCER UNDER LPM

I AM USING STM32 WL55JC2 CONTROLLER TO WORK AS A LORA END NODE , I AM WORKING WITH EXCISTING CODE FOR LORA END NODE AND I WANT TO CONFIGURE UART1 , THE CODE IS WORKING UNDER  SEQUENCER OS. SO I AM TRYING TO IMPLEMENT UART1 WITHIN THE SEQUENCER OS , U...

MANOJ_R by Associate II
  • 2354 Views
  • 4 replies
  • 1 kudos