STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 279 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4104 Views
  • 0 replies
  • 3 kudos

Resolved! LoRa WAN end node development

i am using LoRa E5 dev board for programming my code , i am using STM32 stlink debugger with stm32 cube programmer , the board is not connecting my stm32 cube programmer , the serial number is showing 1 but when i am trying to connect it is not conne...

MANOJ_R1 by Associate
  • 2419 Views
  • 2 replies
  • 3 kudos

Resolved! BLE Data Transfer between TWO STM32WB

I want to configure a stm32wb as BLE central and other as BLE peripheral such that they can exchange data. The combination of all this data also needs to be sent to a mobile phone. Can anyone suggest me a MOOC or may be a document that can  be used a...

Rituraj by Senior
  • 6663 Views
  • 15 replies
  • 4 kudos

adc dma stm32wb55

Im running ble heart of stm32wb55  , I would like use adc input channel with  the  ADC_SingleConversion_TriggerTimer_DMA_ but the tim2 that i instantiate seem not run; the  variable ubDmaTransferStatus that indicate the end of dma tranfert(value = 1)...

Error : Unable to get core ID

Hi everyone,I'm using a Nucleo WL55JC1 trying to run the Lorawan AT_slave application. When trying to run the project in STM32CubeIDE, I get the error "no device found on target". Did the process of the solution on this post : https://community.st.co...

mrgcap by Associate
  • 14743 Views
  • 4 replies
  • 2 kudos

[BLE] User Description Descriptor for a Attribute

I would like for my services and characteristics to have a user readable string name.(when someone discovers them)How do I set that name in the descriptor of the attribute?Is there a convention on how the descriptor need to be set so devices will sho...

DS.4 by Senior II
  • 1716 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.