STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

STM32WB55 BLE LLD DataRate

I am trying to get BLE_LDD_DataRate demo to work, it just sits there with nothing different from pressing SW1 on 1 board and SW2 on second.  Don't have a 3rd board at the moment.The description seems to indicate LED's will toggle, but nothing.I know ...

Resolved! Opus codec with STM32WB5MMGHTR

Hi,I have been trying to add opus codec in my project. But I cannot able to build after adding the opus file. If anyone successfully added opus with their project help me out. I mostly get errors on 'Neon' which is used for FFT. As I searched neon is...

LR.2 by Associate III
  • 11599 Views
  • 18 replies
  • 6 kudos

Multipoint to point communication

Hi everyone, I want to use 50 sensor device and 1 base station. I look stm32wl topics and I can't find the way. I watch hands on tutorial MOOC - STM32WL workshop - 4 Point to point Phy layer application lab. He really well explained for beginners (I...

AHakk.1 by Associate III
  • 4109 Views
  • 9 replies
  • 4 kudos

Resolved! CAP_Init return BLE_STATUS_OUT_OF_MEMORY

Hello    My Project is based on STM32WBA55G-DK1 to develop my ble headphone.But when i called CAP_Init API, it returned BLE_STATUS_OUT_OF_MEMORY. I don't know which parameter is causing this issue. Following Parameters are my ble config. #define CFG_...

Xiaojie by Associate III
  • 2255 Views
  • 4 replies
  • 0 kudos

S2LP WMBUS SMPS VOLTAGE

Hello;My Name is FATIHI am using Wireless MBUS water meter scanning using S2LP and STM32L073. While making the PCB design, we applied the reference design value in the x-nucleo-s2868a2_schematic.pdf file exactly. However, although we see VDD voltage ...

FATIH55 by Associate
  • 1110 Views
  • 1 replies
  • 1 kudos

BLE P2P connection problem.

HiI am using USB DONGLE board (MB1293C) as client and Nucleo board (MB1355D) as server.The BLE_p2pClient application is downloaded in a USB DONGLE board and the BLE P2P_Server application is downloaded in a Nucleo board.My problem is that most of the...

YasinYelkovan_0-1718881097762.png

Resolved! STM32WB ADC not working along with BLE

Hello, I am trying to read battery voltage within a task called by sequencer on STM32WB55CEU.I am following this post: https://community.st.com/t5/stm32-mcus/how-to-use-the-stm32-adc-s-internal-reference-voltage/ta-p/621425I verified that I can measu...

mx1.png a4d5ed2f-c2e3-47ee-b054-d171b82f8b44.png mx2.png