STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 228 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4071 Views
  • 0 replies
  • 3 kudos

STM32WB15cc - Adding custom Characteristics

Hi,I am trying to make a simple BLE service with a custom characteristic descriptor and UUID (128 bit) has anyone got any good examples of this?The reason I ask is when I running a BLE server to advertise the characteristics always just seem to show ...

PLee.3 by Associate III
  • 1196 Views
  • 1 replies
  • 0 kudos

How to use STSAFE-A110 for LoRaWAN ?

Hi, I'm trying to use the STSAFE-A110 to store my LoRaWAN keys, to generate session keys and to encrypt my payloads through it.I'm supposed to send commands to the secure-element but for the symetric encryption, neither the datasheet nor the source c...

Hiraks by Associate
  • 1685 Views
  • 2 replies
  • 0 kudos

Resolved! LoRa operability in other countries

Hello,Our IoT product is LoRa based, and uses the STM32WLE5JC mcu. For the purpose of operability in several countries, we have used a Molex antenna, which operates in the frequency range 863MHz to 928 MHZ.We're using the STM32CubeIDE for development...

Resolved! STM32WB5 BLE

Hi all,no experience, so please explain like to a child.I want to jump into digital.My idea is to make a bluetooth speaker with LED meter so:USB C for Power(CYBD3177) and/or Audio IN(STM32wb5).Bluetooth Audio IN (STM32WB5) -> out to Class D Amp (TAS5...

stop by Associate II
  • 2821 Views
  • 4 replies
  • 0 kudos

Resolved! WB55RG/WB15CC and PLC01A1

Is NUCLEO-WB55RG/WB15CC compatible with X-NUCLEO-PLC01A1? I want to develop a controller that supports BLE and thought of starting with a combination of these two boards. Would be helpful if someone can confirm that these boards are compatible and ca...

TLans.1 by Associate II
  • 1663 Views
  • 1 replies
  • 0 kudos

Implementation of BLE_Hid in STM32CubeWB

Hello. Thanks again for all your appropriate assistance.I would like to ask a question about the implementation details of BLE_Hid in STM32CubeWB.> Is the data written by aci_hal_write_config_data saved in NVM area?(Is that implementation already in ...

ELEHM by Associate II
  • 1462 Views
  • 2 replies
  • 0 kudos

Flash Write Errors on STM32WB with BLE Stack

Hi, I use an STM32WB with the BLE stack. In my code, I need to write data to the flash memory (writing new firmware to a prepared memory area). Unfortunately, when I attempt to write to the flash, an error occurs. Is there anything special that I nee...

JR2963 by Senior II
  • 1882 Views
  • 3 replies
  • 0 kudos

Resolved! Problem flashing a card STM32WBA55G

Hi,  I have a STM32WBA55G card and I want to flash an example code but it doesn't work. So I used STM32Programmer to find out why my board wasn't "found". Normally STLink is included and I can go through the usb-c port. But I still get an error if I ...

Clemint by Associate II
  • 3617 Views
  • 3 replies
  • 0 kudos