STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 228 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4071 Views
  • 0 replies
  • 3 kudos

Resolved! Setting up TouchSensing library

Hi there, I'm currently trying to setup the STM32_Touchsensing library.I have already downloaded the library fromST(https://github.com/STMicroelectronics/STM32CubeWB/blob/master/README.md#how-to-use). How do I enable this Touch sensing library now th...

Parry by Associate II
  • 3558 Views
  • 6 replies
  • 0 kudos

Resolved! Can Stm32wb55 use a hse clock source other than 32mhz?

According to page 118 of stm32wb55ce frequency needs to be exactly 32 mhz with no option of holding any other value at all. However when in stm32cube ide the clock configuration tool lists 4-48 mhz as acceptable input frequency for HSE.Is the datashe...

энн by Associate II
  • 2100 Views
  • 3 replies
  • 1 kudos

Resolved! STM32WB55 EXTI + BLE Low power

Hello,I am using STM32WB55CEU6, when using EXTI callback with BLE and LPM enabled, the MCU never enters the desired STOP2 power mode. The callback triggers every 20 seconds and is used to set a task by calling  UTIL_SEQ_SetTask(...).When a virtual ti...

Resolved! STM32WB set CPU sleep for low power consumption

Hi,I use an STM32WB chipset for my device and my application reads sensor data and sends over the BLE when the device is connected. When the device gets disconnected then after 30 seconds it should STOP BLE advertisement and RF also, go to CPU sleep ...

Resolved! Connections

Hi, new to microcontrollers, I want to use an STM32WBA54 for the BLE and have it control: a class D amp, a Led strip  What I need at this moment is to understand the connections I need in order to have the chips comunicate and work with each other. O...

stop by Associate II
  • 1377 Views
  • 1 replies
  • 0 kudos

Resolved! Nucleo-WBA52CG STM32CubeMX Suport

Hi All, I am trying to get a custom BLE and MEMS project running on the Nucleo-WBA52CG board - however looks like the STM32_WPAN middleware does not work properly also in the latest WBA software pack the applications folder for the board does not hav...

JShro by Associate III
  • 3627 Views
  • 7 replies
  • 2 kudos