Skip to main content
Ugilten
Associate III
August 2, 2023
Question

STM32WB10 CPU2 not responding when exiting standby or shutdown

  • August 2, 2023
  • 1 reply
  • 1718 views

Hi,

I have made an application on that needs to enter shutdown/standby mode on the STM32WB10 MCU.

I have successfully made it enter the shutdown mode, and I can wake it back up again.
However, when it wakes up, it does not get any response from CPU2.
It is as if the task "shci_user_evt_proc" is never called in a way that allows it to call "

APPE_SysUserEvtRx()" in app_entry.c

As a result I only have Bluetooth when the MCU is started the first time from a power cycle.

 

The current version of my application enters standby/shutdown after 10s of no user interaction.
After wakeup, it enters HardFault_Handler() when it attempts to enter shutdown again.

This happens when it attempts to send the command for disabeling the advertising (which i suspect is obvious, since the CPU2 is not responsive).

Below is a screenshot of the stacktrace and the line that causes the hard fault.

Ugilten_0-1690965820287.png

I suspect this is caused by my code not doing something the way it should, but I cannot figure out what it should do, or when.

I have tried unchecking the option byte that resets the SRAM2 when a reset occures, this did nothing.
I have tried to disable BLE when booting from wakeup by running this

 

void DisableBle()
{
	uint8_t rfResetStatus = (RCC->CSR & RCC_CSR_RFRSTS) != 0U ? 1 : 0;
	LL_APB3_GRP1_ForceReset(LL_APB3_GRP1_PERIPH_RF);
	while(!rfResetStatus)
	{
		rfResetStatus = (RCC->CSR & RCC_CSR_RFRSTS) != 0U ? 1 : 0;
	}
	RCC->CSR |= RCC_CSR_RMVF;
}

 

 That did nothing.

 

The ResetCPU2() function that attempts to stop the advertising looks as this

 

void ResetCpu2()
{
	/*stop adv , stop ble stack , reset cpu2 */
	// Stop Advertising
	hci_le_set_advertising_enable(0);

	// Reset the stack
	aci_hal_stack_reset();

	// Reboot CPU2
	SHCI_C2_Reinit();
}

 

 

Can anyone point me in the right direction as to what I am doing wrong?

This topic has been closed for replies.

1 reply

Associate III
February 29, 2024

Hi, I've exactly the same problem. Does anybody have a fix ?

Coco_0-1709207544454.png