STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

BLE MESH ADDING Services

I have two stm32wb5mm dk configured as mesh server and client . I used example  BLE_MESH_MODEL_SENSOR. Can someone tell me what file mentions the data that is being sent and how can I add external sensor or a way to add external service so that it ca...

Rituraj by Senior
  • 973 Views
  • 1 replies
  • 0 kudos

STM32WB55RGV6 No St-Link Detected

I've been struggling to connect my nucleo board via ST-Link, I've tried uninstalling everything, reinstalling and my computer still won't detect the board when I plug it in. It's always just COM-3 device or whatever port I use. Tried installing the S...

jvu by Associate II
  • 4289 Views
  • 9 replies
  • 0 kudos

STM32WB55x LiPo Battery Voltage read in Low Power Mode

Hello, I'm doing BLE usb doungle product.I want to use the WB55RGV6 in low power mode. The system will be able to operate on battery. I have some questions about product development. Questions on below.     1) Can the product operate at 1.8V in low p...

BATTERY READ.PNG
GkhnGmc by Associate
  • 1532 Views
  • 1 replies
  • 0 kudos

stm32wl55jc1

hello everyonei try to make same ping pong dual core example but my project not working can you help me to found the problem"there is not fault in build and i can run the project but it not working"i did not understan where is the problem

STM32WL and STM32WB in the same project

I am working on a battery operated design which utilizes the WB as the main logic CPU with a WL to connect to LoRa networks.   This device is very small, putting the antennas uncomfortably close together.  To avoid certification issues wed like to en...

dovoto by Associate II
  • 2999 Views
  • 4 replies
  • 2 kudos

Resolved! Writing/Erasing internal flash during BLE connection

Hi all, We would like to perform write/erase actions in internal flash during active BLE connection for a slave/peripheral device. We intend to use BLE_RfWithFlash example. We are trying to establish sufficient conditions for a slave to perform write...

oguzcan by Associate
  • 1673 Views
  • 2 replies
  • 0 kudos

STM32WB55 Reconnection issues, event not triggered

Hello community,I am running a modified version of the p2p_routeur_app example and everything is running smoothly except for some rare reconnection issues. The peripheral is a remote control that sends a lever signal to the central and often the peri...

ALedi.1 by Associate III
  • 1867 Views
  • 2 replies
  • 0 kudos