User Activity

HiI`m working on a customised STM32WB55 board and trying to implement eeprom emulation.According to AN4894there should be a BLE_HeartRate_EEPROM_Emul example somewhere but looking at STM32Cube_FW_WB_V1.12.0 package I can`t find it. I have also checke...
HiI have this strange problem which manifest itself using headless build and also inside CubeID when I git clone my project for the first time.Build Settings : I have 4 custom build configuration. I also removed Debug and Release configurations that ...
HiI have a strange problem with my p-nucleo board(MB1355C)Using the example as reference DFU_Standalone (STM32Cube_FW_WB_V1.12.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\USB_Device\DFU_Standalone)I am able to jump to bootloader and perform DFU upda...
HiI`m using PNUCLEOWB55 Board for testing USART1 interrupt communications.I have started a project from scratch using CubeID 1.10.1 and choosed PA9 and PA10 as TX/RX respectively with following configuration 115200Baud, WordLen 8bits(including parity...
Kudos from
Kudos given to