User Activity

Dear ST team, I have an issue with starting the USB bootloader with the STM32WB5MMG-DK and I am sure it is for lack of knowledge. The AN2606 states the following: and USB pins should be able to function as the following:The pattern 16 looks like like...
Hi everybody, how can the CPU1 of module STM32WB5MMG be waken up by the RF subsystem?The idea in mind is to use the module as a BLE Server, have the CPU2 perform advertising while the CPU1 is in STOP2 mode. According to the reference manual RM0434, t...
Hi everybody, I have been looking for the charateristics (like ppm/temperature dependency) of the LSE crystal included in the STM32WBMMG, but I have not been able to find on its datasheet.Is there another document I am missing where the information a...
Hi all, I think this is a bug of CubeMX. Everytime the .ioc gets updated for the project, the code written for the descriptor characteristics get deleted in the SVCCTL_InitCustomSvc() of the autogenerated custom_stm.c file.I don't know if this issue ...