NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Has anyone encountered the issue that external loader works fine only when flashing QSPI EFlash_Section independently (e.g. slice the firmware.elf into MCU.bin and EFlash.bin and flash separately).BUT if flash from 0x08000000(Complete Firmware) the ...
Hello,Our IoT product is LoRa based, and uses the STM32WLE5JC mcu. For the purpose of operability in several countries, we have used a Molex antenna, which operates in the frequency range 863MHz to 928 MHZ.We're using the STM32CubeIDE for development...
Hi all,no experience, so please explain like to a child.I want to jump into digital.My idea is to make a bluetooth speaker with LED meter so:USB C for Power(CYBD3177) and/or Audio IN(STM32wb5).Bluetooth Audio IN (STM32WB5) -> out to Class D Amp (TAS5...
Is NUCLEO-WB55RG/WB15CC compatible with X-NUCLEO-PLC01A1? I want to develop a controller that supports BLE and thought of starting with a combination of these two boards. Would be helpful if someone can confirm that these boards are compatible and ca...
Hello. Thanks again for all your appropriate assistance.I would like to ask a question about the implementation details of BLE_Hid in STM32CubeWB.> Is the data written by aci_hal_write_config_data saved in NVM area?(Is that implementation already in ...
Hi, I use an STM32WB with the BLE stack. In my code, I need to write data to the flash memory (writing new firmware to a prepared memory area). Unfortunately, when I attempt to write to the flash, an error occurs. Is there anything special that I nee...
Hi, I have a STM32WBA55G card and I want to flash an example code but it doesn't work. So I used STM32Programmer to find out why my board wasn't "found". Normally STLink is included and I can go through the usb-c port. But I still get an error if I ...
I have configured a BLE MESH with two nodes one as client and other as server . It is working well . I also want to recieve the same data that is being exchanged on Phone. Can someone tell me how this can be done and what app I must use.
I bought ST-LINK/V2 from a certified reseller, and I have WIO-5E mini with STM32WL5JC from [Seeed.com](https://Seeed.com) on the board. This WIO-5E was already programmed by another ST-LINK/V2. I connected WIO-5E to ST-LINK as required. I want to rep...
I try to debug on a STEVAL-IDB011V1 with WISE Studio.Whatever I try with any project, I have the same error when the debugger tries to launch:Open On-Chip Debugger 0.11.0+dev-00062-g6405d35f3-dirty (2021-03-26-11:44)Licensed under GNU GPL v2For bug r...