STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

CMWX1ZZABZ (STM32L0) external reset issue

Hello,I have a custom board, equiped with a Murata CMWX1ZZABZ, running a firmware based on the LoRa and SigFox libraries provided by ST. Several hundreds, if not thousand, units are currently depoyed. For the most part, everything is fine.See the att...

VinceWnt by Associate
  • 1322 Views
  • 1 replies
  • 0 kudos

Resolved! Where can i find Hands-on_WS_WBA55.ioc file?

Hello,i want to start a Project based on Hands-on_WS_WBA55.ioc file, as descriped in STM32WBA5x Workshop - 4.But i only find on github the Hands-on_WS_WBA52.ioc file.Where can i download the file Hands-on_WS_WBA55.ioc?  

ledi7 by Associate III
  • 1439 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55CG Zigbee connection Tuya Smartlife with ST Example

Hi together,I have the STM32WB55CG on a custom PCB and plan to integrate it into a smart home Zigbee network, that uses a Tuya Gateway and is controlled by Smartlife app. I tried to use the project Zigbee_Find_Bind_OnOff_Router1 from the ST examples ...

vh789 by Associate III
  • 1683 Views
  • 2 replies
  • 1 kudos

Resolved! Board support package

I have a very generic question ,What happens if in an example for a different board . I just remove the BSP and instead add a BSP for a different board.

Rituraj by Senior
  • 1846 Views
  • 4 replies
  • 3 kudos