cancel
Showing results for 
Search instead for 
Did you mean: 

Cell selection at 100 to 300mAh, Li ion, Li Polymer or LiFePO4

David_
Senior

What are pro and con?  Re-charge cycle few days to few weeks.  STM32WLE5JC. TIA

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @David_ 

For the battery, i suggest you to select the best one according to the life cycle, price, ... Also, for the recharge cycle, it should be up to few weeks but it depends on your application, the features that you are going to use, the low power modes,....

So the best way is to test you application to now what the exact Re-charge cycle.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @David_ 

For the battery, i suggest you to select the best one according to the life cycle, price, ... Also, for the recharge cycle, it should be up to few weeks but it depends on your application, the features that you are going to use, the low power modes,....

So the best way is to test you application to now what the exact Re-charge cycle.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.