NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,i am using STM32WBA55 with BLE_p2pServer_ota example and want to wake-up over an USART2 event (start bit or rising edge) from stop mode. What is a good way to do this? I am using HSI16 with USART2 GPDMA1.
I'm trying my hand at a LoRa project and settled on using the STM32WLE5JC chip on Seeed studio's Wio-E5 module. I've read through the bootloader manual and Seeed studio has their own set of instructions for wiping their pre-existing code which I have...
I've been using B-WB1M-WPAN board with a modified example of motion service from BLE_HR_p2p_Sensor. but with IMU readings with a steval-mki217v1 shield connected with SPI. I already have the CRC checked from CubeMX generation. So far I have been ab...
Hello For the Nucleo STM32WB05KZ board, the transmission power is normally 0 dBm by default (it can go up to 8 dBm). Is it possible to modify the transmission power according to my needs, for example to 3 or 4 dBm, using STM32CubeProgrammer or ano...
On this page: https://www.st.com/en/microcontrollers-microprocessors/stm32wle4c8.htmlThe device is specified as having LoRa support in the first paragraph of the description but lower down in the "More from the product line" section the WLE4 chips ar...
I'm building an application for a BlueNRG-LPS (332), now rebranded as STM32WB05TZ (WLCSP-36 Package) by starting with a simply Blinky project testing the clock signals of my device. I need to enable the PLL64M clock source to use the radio peripheral...
Hello,I'm working on a project started from Zigbee_APS_coord and Zigbee_APS_router examples on NUCLEO-WB55.USBDongle with STM32Cube_FW_WB_V1.21.0.The project is based on data exchange between the coordinator and several devices acting as routers (fro...
Hello, I'm working on a project started from Zigbee_APS_coord and Zigbee_APS_router examples on NUCLEO-WB55.USBDongle with STM32Cube_FW_WB_V1.21.0.The project is based on data exchange between the coordinator and several devices acting as routers (fr...
Hello STM Community ,I am designing an internal PCB antenna for LoRa communication using the STM32WL55JCI7 at EU868 frequency. Is a PCB antenna recommended by STM for this chip? If so, what guidelines or procedures should I follow for designing a PCB...