STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! Not able to get BLE working on STM32WB55CGU6

Hello,I'm trying to get BLE working on my custom STM32WB55CGU6 board. I was following this tutorial since it matches well with my setup: STM32 Bluetooth Firmware Tutorial (Bring-Up) - Phil's Lab #129However I am not able to see my board using nRF Con...

Jaws404_0-1742200932945.png
Jaws404 by Associate II
  • 2620 Views
  • 6 replies
  • 1 kudos

STM32WB55CEU6 SDMMC or other options

Hi all,   We want to use STM32WB55CEU6 for a project that needs wireless transmission, but at the same time we would also like to have onboard memory in form of a micro SD card. What I have found so far is that STM32 products integrate SDMMC controll...

Looking for Nucleo-WB05KZ BLE example

Hello, i'm starting with the Nucleo-WB05KZ for the first time, i found some exemples (hex files) to test, please have you un exemple just to try the BLE communication between the board and android application : exchange of data for exemple ?  thanks 

ljm by Associate III
  • 1192 Views
  • 3 replies
  • 0 kudos

DHT22 Sensor with LoraWan stack

Hi, I'm trying to implement a DHT22 humidity/temperature sensor in the Lorawan stack. The stack works fine, as does the sensor, but separately. When I try to combine them so that each time I send the data, the sensor reads it, they don't work.

dvid by Associate II
  • 6374 Views
  • 15 replies
  • 2 kudos

Resolved! STM32WB FUS by CubeProgrammer GUI and CUI

If I tried to connect Nucleo-WB55RG with CubeProgrammer GUI and CUI to update wireless stack using swd connection, the behavior of each was different.I could start FUS and update wireless stack on GUI, but cannot start FUS and update wireless stack l...

スクリーンショット 2025-03-13 175958.jpg スクリーンショット 2025-03-13 180036.jpg
mtahara by Associate
  • 1328 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB55 IrDA hardware setup

after looking over all the documentation i could find (datasheet, reference manual, etc.), i could not clearly find how i am meant to connect IR LED(s) for IrDA communication with an STM32WB55. The image i attached is a screenshot from the reference ...

Tvan .15 by Associate
  • 7799 Views
  • 4 replies
  • 1 kudos