Pin sharing problem with SWD and SPI3, GPIO
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-16 1:09 PM - edited ‎2025-01-16 1:12 PM
Hi. I'm developing a custom board using STM32WB09TEF7TR microcontroller.
I had a problem re-accessing the microcontroller using SWD once I finished programming one time.
I found that it is due to the SPI3 (PA3) and one GPIO pin (PA2) sharing the pin for SWD (SWCLK and SWDIO).
So, I want to control this microcontroller with two stages, "operation mode" / "programming mode", that change the pin setting from SPI3 / GPIO_out to not assigned pin for SWD.
Could you tell me what I can do about this?
I failed to change the pin setting using the function below.
void enter_SWD_mode(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = SYNC_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(SYNC_GPIO_Port, &GPIO_InitStruct);
APP_DBG_MSG("SWD Mode activated.\r\n");
}
Solved! Go to Solution.
- Labels:
-
STM32WB0 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-20 9:23 AM - edited ‎2025-01-20 9:24 AM
This problem is solved by skipping MX_SPI_init() and MX_GPIO_init() in the main function.
Instead, the two functions are called before actual use.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-20 9:23 AM - edited ‎2025-01-20 9:24 AM
This problem is solved by skipping MX_SPI_init() and MX_GPIO_init() in the main function.
Instead, the two functions are called before actual use.