NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
When I use the IDE to configure USART1 in Half-Duplex mode, the GPIO setting is wrong.Indeed, PB7 is set instead of PB6.Also, its mode is set to GPIO_MODE_AF_PP instead of GPIO_MODE_AF_OD.This cannot be changed from the IDE/MX configuration wizard, u...
I'm using the P-NUCLEO-WB55 development board, with only USB (CDC Device) and USART1 enabled/configured through the STM IDE.The code is generated, I add my own code, I compile, program, test it, and everything works.However, whenever I close and open...
Hello everyone,I am working on a project on which i would like to send a notification from a board to another when the firts one crosses a threshold with the built-in comparator. I started from the BLE_p2pServer and BLE_p2pClient examples from STM32C...
Have the STM32WB Dev Kit schematics been published anywhere?
Hi, I'd like to know how to use a STM32WB Dongle as central to interface a PC windows App to communicate with a STM32WB DK. Are there any examples I can use as a starting point?
Just got this Nucleo pack, the Nucleo board flash cannot be erased or programmed with CubeProgrammer or EWIAR app. I followed exactly the STM32CubeWB Getting Started Guide - can someone tell me how to program the flash please? Also the USB Dongle i...
Firstly I'm very new to all of this so apologies if this is trivial.I have been trying to debug and run a simple blinking led project onto a STM32WB nucleo board using the STM32CubeIDE v1.0 (MacOS). After staring the debugging session, the console di...
Is it possible to use STM32WB as NCP (network co-processor device) for border router in Thread network?
The answer from the processor isRSS state is WIRELESS_STACK_UPGRADE_ONGOINGRSS status is RSS_IMAGE_NOT_FOUNDRSS state is RSS_IDLERSS status is RSS_NO_ERRORFirmware Upgrade process started ...Updating firmware ...Firmware update finishedFirmware Upgra...
error message: [E] DeviceEmdWrapperIcm20649: timeout while waiting for response [E] DeviceEmdWrapperIcm20649: timeout while waiting for responseGot 'Timeout, action did not complete in time: EmdWrapper firmware did not start properly' exception whil...