STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Build For Internal SRAM

Hi,I am trying to reconfigure my project based off the STM32H750B-DK to run on the same part but from a custom PCB. I am using IAR and EWARM. I have configured my icf file based on what I would like for a memory map. The project builds okay, and I ca...

belair55 by Associate III
  • 3086 Views
  • 3 replies
  • 0 kudos

Can we get to modify the code templates?

TouchGFX generates incorrect code that will not compile. Even though a small fix is indicated, I cannot get touchGFX to leave the correct code alone and compile the project.The error I get is  In file included from TouchGFX/generated/gui_generated/sr...

shorai by Associate III
  • 1202 Views
  • 2 replies
  • 0 kudos

Blinking dots problem

Hi,I am using TouchGFX 4.10 with STM32F769 on a custom board. My graphics includes 2 archs and 2 gauges  (added as png)  that must be rotate and two counters in the format HH:MMWhen the system is active, counters must have  “:�? blinking  @2Hz and  g...

d.v. by Associate II
  • 2048 Views
  • 4 replies
  • 0 kudos