STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

White boxes when using Fonts from External Flash

This is a project that I just updated from TouchGFX 4.5 to 4.19.I've been working to update a project to use external flash fonts instead of internal which was the reason from upgrading from 4.5 to 4.19.I'm stuck at a point where the font gets loade...

0693W00000SvTbvQAF.png
JGoew.1 by Associate II
  • 4151 Views
  • 8 replies
  • 0 kudos

Exporting Crank Storyboard GUI to STM Cube IDE.

I am trying to export a project from Storyboard to Cube IDE. I have seen a few tutorials through IAR IDE but have not seen aby regarding Cube IDE. I have exported the header file from storyboard, but am at a lost at what to do next.

MAlan.1 by Associate III
  • 926 Views
  • 0 replies
  • 0 kudos

Resolved! How to disable slider programmatically?

I have a setting which can be manually or automatically adjusted/changed. A toggle button selection choses manual or automatic adjustment. Manual adjustment is done using a slider widget. When the toggle button is selected to automatic position, slid...

BGuth.1 by Senior
  • 2222 Views
  • 2 replies
  • 0 kudos

Now, we can get current consumption on the LCD display. However, when we connect the board with PC via 5 different Micro USB cables with STM32CubeMonPwr software (in two different PC with windows 10 system). Both 2 PC cannot SELECT BOARD in STM32CubeMonPw

Now, we can get current consumption on the LCD display. However, when we connect the board with PC via 5 different Micro USB cables with STM32CubeMonPwr software (in two different PC with windows 10 system). Both 2 PC cannot SELECT BOARD in STM32Cube...

JZhon.11 by Associate
  • 1829 Views
  • 2 replies
  • 0 kudos

Stm32CubeIde data mismatch

Hello,I am trying work with the demo of touchgfx designer with my stm32g071rb and the x-nucleo-gfx01m2.The example project works fine if I flash it via TouchGFX designer.When I import it in stm32cubeide, after setting up the external loader found in ...

lpado.1 by Associate
  • 3790 Views
  • 8 replies
  • 0 kudos

Resolved! Space character displays as Fallback character (bug?)

Hi!In my project I added a text area with one wildcard. I checked option "Use wildcard buffer", but left "Initial value" blank. Then in setupScreen() function I wrote some text to the wildcard buffer using Unicode::strncpy(). After starting my projec...

ypiotrp by Senior
  • 4683 Views
  • 6 replies
  • 1 kudos