STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX Widget TextArea Alignment

I have set up some TEXTS (On Off). I noticed that there are 2 alignment settings here (see #2 and #3) in the imageWhat does the 2 alignment setting do?Then there is the alignment for the actual widget (#1)Which alignment wins as far as the text being...

Resolved! How can I create a TouchGFX Project with the STM32H7B3I-DK and write usercode with CubeIDE?

I have start with TouchGFX, select the demo board and generate the code. Simulator and download works.But now, when I want open the project with CubeIDE, the first is, the project is completly empty. Then when I start a new project with the existing ...

MMüll.6 by Associate III
  • 5234 Views
  • 11 replies
  • 0 kudos

Resolved! How to solve the Enum in struct build error

Not sure what I am doing wrong here in my header file. I have a struct pump_info which has some enums as properties. I get a build error on all 3 on the enums in the struct. Error'operation_mode' does not name a type'operation_mode' does not name a t...

SBSFU & Touchgfx ->Firmware signature check failure.

Hi all,SBSFU ported to many custom boards and in projects, and is working as expected. But in a project with Touchgfx throwing error "error was: Firmware signature check failure." on Installing update FW from download area.As it is working for other ...

JChou.1 by Associate III
  • 1713 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX with STM32H745I_DISCO

I try to make an application with STM32H745I_DISCO. After I enable TouchGFX, and generate code, the project fails to compile.Did ST started supporting TouchGFX officially on STM32H745I controllers ?Is there any official documentation/guidelines ?If a...

NSeba by Associate III
  • 4087 Views
  • 7 replies
  • 0 kudos