STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Touch GFX with SPI Display.

Hi Community,I have followed the following link https://www.youtube.com/watch?v=suMytEyQTP4&t=774s and got the output (SPI display interfacing with Touch GFX). Now I wanted to use the single framebuffer strategy to get the same but no output. So, an...

Vins by Senior
  • 1648 Views
  • 2 replies
  • 0 kudos

Resolved! Stop getting two gesture events from one gesture

On a screen, I use the function handleGestureEvent. Inside this function, I have an if-else to differentiate between horizontal and vertical swipes:void handleGestureEvent(const GestureEvent& event) { if (event.getType() == GestureEvent::SWIPE_HO...

Pirol by Associate III
  • 3016 Views
  • 6 replies
  • 0 kudos

Adding canvas "containers" at run-time

For a job commissioned by a client, do I need to add a widget on a page to Run-time.If I don't find a solution, I'm forced to abandon TouchGFX (which I find very versatile), and migrate to another platformIs there an example?Is there any documentatio...

DDi S.1 by Associate III
  • 1906 Views
  • 3 replies
  • 0 kudos

Hello, I have initialized 2 layers on my stm32f429. I want to make the second layer which is an image with resolution 274*184 to be written line by line: here is my code ...Can you help me to do it? when I compile the code, it loads immediately.Thanks

LTDC_InitTypeDef LTDC_InitStruct; LTDC_Layer_InitTypeDef LTDC_Layer_InitStruct; Delay_us(2000000); LTDC_LayerCmd(LTDC_Layer2, ENABLE); LTDC_ReloadConfig(LTDC_IMReload); for(int i=0;i<=184;i++){ Delay_us(1000000); LTDC_Layer_InitStruct.LTDC_CFBLineN...

nsabo.1 by Associate II
  • 1003 Views
  • 1 replies
  • 0 kudos

Setup TouchGFX with SPI display, ILI9341. Partial Buffer project will not work on cubeIDE but works in KEIL.

The project in youtube https://www.youtube.com/watch?v=suMytEyQTP4&t=616sis not working in cube IDE. I tried it using cubeIDE v1.10.1, GFX v4.20.0, cubeMX v6.6.1. The code compiles no errors. But the TFT shield is blank ! Can you help resolve this us...

0693W00000QLoRhQAL.jpg 0693W00000QLoRXQA1.jpg
ksale.1 by Senior II
  • 1609 Views
  • 1 replies
  • 0 kudos