STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

EMWin Serial Interface

I would like to control a qaurter VGA display with an ST7789V controller with just the serial (SPI) interface since the parallel bus is not connected. How do i achieve this in STM32Cube, it lets me only select parallel or DSI modes with an STM32F4xxT...

MHaub by Associate
  • 741 Views
  • 0 replies
  • 0 kudos

How to program the TFT LCD in stm32f429?

hi nerd fellows, I got a new task from my superior that I need to program the TFT LCD in stm32f429 discovery development board. I had no idea what to do because I am totally a beginner at this. help me out ??

Ark1 by Associate II
  • 6390 Views
  • 4 replies
  • 0 kudos

STM32F429-Discovery landscape display

Posted on November 12, 2013 at 17:12Good morning,i have a problem with display orientation, i have changed the ili9341 register and the image rotate correctly but, i have a white portion of the display of 80 column in the side of the display.the LTD...

STemwin hard fault if buffer in ext sram.

Hello,I have a project based on STM32F417ZET. I want to use the STemwin library (STemWin532_CM4_OS_GCC.a) provided by ST. I'm using FreeRTOS that's why the lib is the _OS_ version.Two things attached to the uC via FSMC:external SRAM type: IS66WV51216...

PBalo by Associate
  • 1378 Views
  • 1 replies
  • 0 kudos