STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

DSI display interface doesn't work

HiI'm development a board with STM32F779a cpu connect with dsi display.I create the graphic wit TouchFX tools and included in the STM32cube ide design software.How example I see STM32f769i-disco demo, and received the init code of display by producer...

PZamb.2 by Associate III
  • 11280 Views
  • 13 replies
  • 0 kudos

How to resolve this error?

13:05:53 **** Build of configuration Debug for project C7 **** make -j12 all arm-none-eabi-g++ -o "C7.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"C:\Users\martynasveit\Desktop\C7_2(20230226)\C7_SVN\STM32H743ZITX_FLASH.ld...

heyo by Senior
  • 2684 Views
  • 6 replies
  • 0 kudos

TouchGFX absolute minimal sized build

I want to implement a bare bones TouchGFX bootloader application that provides text based feedback for status & %programmed. The idea is for the bootloader to be in FLASH sector0 and for it to be able to program a more complex TouchGFX based applicat...

dave2012 by Associate III
  • 1041 Views
  • 0 replies
  • 0 kudos

Resolved! Touchgfx files with C only!

Every project generated from TouchGFX Designer is based on C++ (file .cpp). Is there a possibility to have project generated from TouchGFX Designer based on C only (file .c)?Also are there any examples from TouchGFX Designer where the codes are in C?

TouchGFX build project issue

Hello,I am usual of Stm32CubeIde. I try first time TouchGFX V 4.21.3 with H747 DISCO.TouchGFX simulator is well working. But after generating (clicking on the project icon in C:\TouchGFXProjects\MyApplication_1) the project in Stm32CubeIde, the build...

BRobe.3 by Associate III
  • 4371 Views
  • 3 replies
  • 0 kudos

Resolved! Upgrade to TouchGFX 4.21.4 undefined reference

Description Resource Path Location Typeundefined reference to `touchgfx::ConstFont::ConstFont(touchgfx::GlyphNode const*, unsigned short, unsigned short, unsigned short, unsigned char, unsigned char, unsigned char, unsigned char, unsigned char, unsig...

rgree.1 by Associate II
  • 1698 Views
  • 1 replies
  • 0 kudos

Resolved! Adapting Touchgfx codes to bigger LCD screen

I am using Touchgfx for the STM32H745I Disco board. So far it has worked well with the default screen (4.3 inch). But I would like to use a bigger screen. So I will connect the STM32H745I board to a 9 inch screen. Now my question is, will touchgfx co...