STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX support ST7796 or not ?

i have stm32h750vbt6 and i want applied with TFT screen http://www.lcdwiki.com/4.0inch_SPI_Module_ST7796in test demo is work then i don't know can use with TouchGFX or not

non by Associate III
  • 5848 Views
  • 4 replies
  • 0 kudos

Resolved! How it works the return??

Hello all,I'm using the HAL library for the camera, specifically I'm using the function: HAL_StatusTypeDef HAL_DCMI_Start_DMA(DCMI_HandleTypeDef *hdcmi, uint32_t DCMI_Mode, uint32_t pData, uint32_t Length)In the function are many return HAL_ERROR, an...

BTurc.2 by Senior
  • 3197 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFXDesigner without Internet or on linux

My company has strick internet security. So TouchGFXDesigner is not connected to the internet. Can I use TouchGFXDesigner without Internet?So there is another PC installed Linux. Internet security for Linux is not very strict. If possible, I want to ...

sini by Associate II
  • 1880 Views
  • 2 replies
  • 1 kudos